Belimo Damper Actuators, Control Valves, and Sensors
Belimo is Releasing New Room Sensors for a Healthier Room Climate
There will be a virtual launch event on August 30th with Dr. Elena Cortona, Head of Innovation,...
1 minute read
What is an HVAC Retrofit?
An HVAC Retrofit is the process of integrating new components into an older system. Many...
1 minute read
The Benefit of Thermal Energy Metering
With increased energy costs and mandates from government agencies to reduce carbon emissions, it is...
2 minute read
PI Valve Enables Data-Driven Optimization of Shands Hospital
University of Florida (UF) Health Shands Hospital is a top-tier academic medical center. With its...
3 minute read
The Benefit of Electronic Fail-Safe Function in a Cooling Tower
Belimo butterfly valves are designed for various applications, including chilled water, hot water,...
1 minute read
Types of HVAC Communication Protocols
System integrators can take full advantage of field devices' flexible control and data with...
2 minute read
Gas Monitoring in Enclosed Parking Facilities
Mechanical engineers are usually responsible for designing the ventilation system in enclosed...
2 minute read
Smart Building Solutions meet Demanding Requirements for Aesthetics and Functionality
545wyn is a first Class A office building in Wynwood, Florida. Gensler designed the building with...
1 minute read
Increasing Efficiency of Energy Usage in a Building
“The buildings sector accounts for about 76% of electricity use and 40% of all U. S. primary energy...
1 minute read
Topics
- Actuators (12)
- Ball valve (2)
- Belimo News (111)
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
- Green Building Technology (79)