Belimo Damper Actuators, Control Valves, and Sensors
Posts about
Technical Tips (3)
Demystifying the Manual Balance Valve
When it comes to the topic of components in a hydronic piping package, the Manual Balance Valve...
2 minute read
The Effectiveness of Butterfly Valves and Sensors in a Hybrid Free Cooling System
Freshwater is a critical natural resource; we are all more conscious of our water consumption now...
2 minute read
IAQ Control for Healthy, Resilient, Low Energy Buildings
Decades of evidence indicate that current minimum standards for indoor air quality (IAQ) are...
1 minute read
Increasing Efficiency of Energy Usage in a Building
“The buildings sector accounts for about 76% of electricity use and 40% of all U. S. primary energy...
1 minute read
HVAC Strategies to Improve IAQ
Even in a pandemic-free world, there are important reasons to maintain healthy indoor air quality...
2 minute read
Seven Steps to Verify Economizer Performance
Studies have shown that up to 70% of economizers are not functioning correctly. Many economizers ...
1 minute read
The Benefit of HVAC Piping Packages
Piping Packages, sometimes referred to as coil kits or hose kits, are a streamlined method of...
2 minute read
Factors to Consider for Actuation on Large Multi-Section Dampers
When designing commercial HVAC damper applications, many factors are considered that impact...
2 minute read
What is CV, and How Do I Calculate It?
Valve Flow Coefficient (Cv) is the flow capability of a control valve at fully open conditions...