Belimo Damper Actuators, Control Valves, and Sensors
Posts about
Pressure Independent Valves (4)
Belimo Energy Valve Helps Red Wing School District Increase Energy Efficiency
Located in Goodhue County, Minnesota, on the western bank of the Mississippi River, the Red Wing...
2 minute read
Pressure Independent Valves a Good Solution for Water Source Heat Pump Application
In a water source heat pump (WSHP) application, a variable or constant speed pump accomplishes...
1 minute read
Critical Zone Reset Logic Increases Pumping Efficiency
Hydronic variable flow systems may reset supply water temperature, pump static pressure, or a...
2 minute read
District Cooling and the Effects of Low Delta T
District cooling is the centralized production and distribution of cooling energy. Chilled water is...
1 minute read
Belimo Energy Valve™ is Now Solving Low Delta T Leveraging IoT
Belimo Americas is excited to announce the release of the new Energy Valve that is now an IoT...
1 minute read
New Belimo ZoneTight™ Zone Valves - Efficient in Every Way
Belimo Americas is pleased to announce the release of their new ZoneTight zone valves which are...Energy Valve Proves Air Coils are Batting a Thousand
When sports fans crave game highlights or need to check the latest stats and ranking for their...
4 minute read
New Compact Performance Solution that Manages Flow
The new ePIV is a 2-way pressure independent characterized control valve with an integrated...
1 minute read
ePIV Now Available in Sizes ½” to 6”
Belimo releases the Electronic Pressure Independent Valve (ePIV) in sizes of ½” to 6”; a 2-way...