New 6-way Valve Reduces Installation Cost

The 6-way Characterized Control Valve (CCV) is the only one of its kind designed specifically for chilled beams and radiant ceilings. This compact valve has the functionality of up to four straight through valves saving on space, material and installation time.

Achieve Better Control and Cut CostBelimo 6-Way CCV
Belimo 6-way Characterized Control Valves (CCV) feature heating and cooling circuits which are hydraulically decoupled because of the innovative ball design. Each sequence is controlled individually by the rotary movement of the actuator. The valve is bubble-tight in the closed position preventing energy losses and helps reduce operating costs.

The 6-way CCV offers:

  • True close-off to isolate both heating and cooling loops.
  • Two sequences with different Cv capabilities (eg. heatingand cooling)
  • Linear flow characteristic
  • Reduced installation cost by using only one coil for heating and cooling.
  • One valve can support the coil with 2 different Cv values (heating and cooling).
  • One valve performs change over and modulating control.
  • Energy savings in close position.
  • Reduced labor costs during installation.
  • Only one analog output needed to control both sequences.

https://www.belimo.com/mam/americas/technical_documents/Tech%20docs/ccv_technical_document.pdf

 

 

 

Back to Blog