Retrofit Solutions for Replacement of Damper Actuators
By improving the method of installing actuators onto jackshafts, the installer saves on installation time translating into a cost savings. The quicker the install, the sooner the installer can move on to the next project. Now with the ZG-JSL linkage all jackshaft installations will only take minutes!
The ZG-JSL linkage simplifies typical installations and eliminates the difficulties where jackshaft bearings are hard to access. The ZG-JSL linkage has a built-in shaft which allows the direct coupling of Belimo actuators. The anti-rotation plate enables the installed actuator to be rotated 90 degrees for space saving applications.
The ZG-JSL linkage is designed to facilitate the attachment of select Belimo actuators to a damper's jackshaft. The unique open ended design allows the linkage to clamp on to any part of a jackshaft measuring from 1/2” to 1.05” in diameter.
The ZG-JSL linkage transfers actuator torque to the jackshaft. There is a torque reduction when using the ZG-JSL linkage with the following actuators. Ensure application requirements before ordering. Order the actuator and linkage assembled at the factory and save on cost with the ZG-JSLA option.
The ZG-JSL linkage can be purchased as an accessory for a list price of $250.00. Belimo can factory mount the ZG-JSL to any of the actuators shown for a list price of $200.00 plus the cost of the actuator.
5-Year warranty on ZG-JSL linkage when used with a Belimo installed actuator only. Ordering example for ZG-JSL linkage assembled with AMX24-3 actuator: ZG-JSLA+AMX24-3.
A closer look:
The ZG-JSL linkage will be on display at AHR Expo, January 31 to February 2, 2011 at the Belimo Booth N5162, Las Vegas Convention Center, Nevada. Or contact Belimo for more information www.belimo.us.