Belimo Tech Support: Frequently Asked Questions

At Belimo, we take pride in delivering precision-engineered actuators, valves, and sensors that set HVAC industry standards for reliability and quality. However, we recognize that even the best products come with occasional questions, and our commitment to exceptional customer support ensures that you receive prompt and accurate answers. Here, we've compiled the most frequent inquiries our tech support, field support, and inside sales teams encounter, along with clear and practical answers. Whether you're seeking details about actuator installations, valve applications, sensor functionality, or our advanced Energy Valves, this FAQ section is designed to quickly connect you with the insights you need to keep your project running smoothly.

If you have further questions or need additional information, don't hesitate to contact our tech support team. We're always here to help.

Actuators

  1. Can dual AF actuators on the same shaft be wired parallel?
    • No, dual AF actuators on the same shaft should NOT be wired parallel.
  2. Can the new AFB24-SR actuator replace an older dual-mounted AF24-SR actuator?
    • No, the new-generation SR actuators have removed primary and secondary capabilities, so the AFB24-SR cannot replace the older dual-mounted AF24-SR.
  3. Is there a difference in functionality between the AFB24-MFT and AFB24-MFT-X1?
    • No, there is no difference in functionality between these two models. The only difference is that the AFB24-MFT-X1 has a linkage and is designed to pair with a valve.
  4. Can NFB and AFB actuators accept S2A-F US auxiliary switches?
    • Yes, they can.
  5. Can an AFX24-MFT95 be reprogrammed with the PC Tool?
    • No, it cannot be reprogrammed with the PC Tool.
  6. Can the PR actuator be mounted upside-down when used inside or outside?
    • The PR can be mounted upside-down if installed inside with no condensation present. It cannot be mounted upside-down if installed outside.
  7. How can PR series actuators be programmed?
    • They can be programmed with NFC, the PC Tool, or the ZTH Tool.
  8. Can an S1A or S2A auxiliary switch be mounted under the cover of NEMA 4 actuators?
    • Yes, for non-spring and electronic fail-safe NEMA 4 actuators. No, for spring return NEMA 4 actuators.
  9. Are heaters for Belimo NEMA 4 actuators available for individual sale or field installation?
    • No, they are not available for individual sale or field installation.
  10. How should outdoor, vertically mounted NEMA 4-rated actuators be installed?
    • They can be installed with the conduit fittings pointing towards the ground, 9 o’clock position, or 3 o’clock position. They should NOT be installed with the conduit fittings pointing skyward.
  11. Is there a weather shield available for the TR actuator?
    • No, there is no weather shield available for the TR actuator.
  12. Do spring return actuators have an optional terminal strip?
    • No, they do not.
  13. Is there a Belimo equivalent for Honeywell Sylk-enabled actuators?
    • No, there is no equivalent Belimo equivalent for Honeywell Sylk-enabled actuators.
  14. Are factory-installed cables on airside actuators field-replaceable?
    • No, they are not field-replaceable.

Fire & Smoke Damper Actuators

  1. Do Fire and Smoke (FS) actuators come with plenum-rated cables?
    • No, they do not.
  2. Do Fire and Smoke (FS) actuators require maintenance?
    • No, they never require maintenance.
  3. Can Fire and Smoke (FS) actuators be mounted on valves?
    • No, they should never be mounted on valves.
  4. What is the rating of Fire and Smoke (FS) actuators?
    • They are NEMA 1/IP40 rated.

Sensors & Meters

  1. Are Belimo flow meters rated for use in wastewater treatment applications?
    • No, they are not rated for use in wastewater treatment applications.
  2. Are Belimo flow meters rated for use in potable water?
    • No, they are not rated for potable water.
  3. Are Belimo flow meters factory calibrated?
    • They are wet-calibrated from the factory to ensure accuracy.

RetroFIT+

  1. Does Belimo have universal butterfly valve retrofit kits?
    • No, we do not.
  2. Does Belimo have universal globe valve retrofit kits?
    • Yes, we do.
  3. Can the Belimo UGVL linkage be used on both new and old-style Belimo globe valves?
    • No, it cannot.
  4. Should an SGVL linkage be used to retrofit current Belimo globe valves?
    • No, it should not be used.
  5. Do FGVL linkages work on Belimo flanged globe valves?
    • Yes, they do.
  6. Does Belimo have universal ball valve retrofit kits?
    • No, we do not.
  7. Can universal linkages for Belimo linear valve actuators be purchased separately?
    • Yes, they can.

Valves

  1. How should steam valves be piped?
    • Steam valves should always be piped in horizontal piping.
  2. What does Cv mean?
    • Cv is a valve’s flow rating, indicating how many gallons per minute (GPM) of water at 60°F can flow through the valve with a 1 psi pressure drop.
  3. Can the B port on a three-way valve be capped to convert it to a two-way valve?
    • No, a three-way valve cannot be capped to convert it to a two-way valve.
  4. Should the characterizing disc in a Belimo CCV be removed in the field?
    • No, the disc is not designed to be removed at all.
  5. Does Belimo sell a NEMA 4 option for a threaded globe valve?
    • No, we do not.
  6. Does Belimo sell repack kits for flanged globe valves?
    • Yes, we do.
  7. Does Belimo offer a solution for a NEMA 4 flanged globe valve?
    • No, we do not.
  8. Does Belimo sell weather shields for use on the DRCX/DKR?
    • No, but there are NEMA 4X versions of the DRCX/DKR available.
  9. Does Belimo provide special order modulating actuators for 3-way ZoneTight valves?
    • No, we do not.
  10. What Cv rating should be used to select a butterfly valve for modulating service?
    • Use a 60 Cv rating.
  11. Are SY actuators for the new L series butterfly valves?
    • No, SY actuators are for HD series butterfly valves. L series butterfly valves use JR and PR actuators.
  12. Can feedback potentiometers be installed in the field on SY actuators?
    • No, they cannot.
  13. Does Belimo sell Victaulic butterfly valves with manual handles?
    • No, we do not.
  14. Are Belimo VS ball valves WOG (water, oil, gas) rated?
    • Yes, they are.
  15. Can VSS ball valves be used for potable water applications?
    • Yes, they can.

Energy Valve

  1. What usernames can be used to log into the Energy Valve dashboard?
    • guest, maintenance, admin (all lowercase)
  2. What sizes are available for the Belimo Energy Valve 4 (EV4)?
    • ½”, ¾”, 1”, 1.25”, 1.5”, 2”
  3. Does the Belimo Energy Valve need to be installed on the system's return piping?
    • No, it does not.
  4. Did EV3 require a section of straight pipe on the valve inlet to achieve flow accuracy?
    • Yes, it required a section of straight pipe with a diameter 5 times the valve size.
  5. Does the EV4 require a section of straight pipe on the valve inlet to achieve flow accuracy?
    • No, a section of straight pipe is not required on the valve inlet of the EV4 to achieve flow accuracy.
  6. Is there a requirement for a section of straight pipe on the outlet side of the EV3/EV4?
    • No, there is no such requirement.
  7. What modes on the Energy Valve will achieve pressure-independent valve performance?
    • Flow Control and Power Control modes.
  8. Do the Energy Valve, EPIV, and Thermal Energy Meter need to be recalibrated?
    • No, they are wet-calibrated from the factory and do not need recalibration.
  9. Does Belimo offer weather shields for the 4th generation EV/EPIV?
    • We do not offer weather shields for the 4th generation EV/EPIV. However, we provide NEMA 4 rated versions of these assemblies, which offer superior protection compared to weather shields.
  10. Can the EV operate without a control system?
    • Yes, it can.
  11. What is required when installing an Energy Valve on an MS/TP network?
    • A 120-ohm end-of-line resistor must be installed.
  12. What flow characteristic does the Energy Valve follow by default?
    • It follows an equal percentage flow characteristic.
  13. What is the flow feedback (U5) value scale for the EPIV and Energy Valve based on?
    • It is based on V’max.

Belimo Download Center

  1. Where can CAD drawings for Belimo products be found?
    • They can be found at the Belimo Download Center.
  2. Where can installation instructions and product documentation be found?
    • They can be found at the Belimo Download Center.
Back to Blog