Why Economizing Makes Sense
Energy usage typically represents a significant portion of a company’s total operating costs, and in a day and age when sustainability and efficiency are at the forefront of industrial design, the demand for innovative products and methodologies that can cut energy expenditures is becoming increasingly prominent.
Economizing provides a wide range of energy-related benefits and with a number of recent technological advances in the design of economizers over the past few years, they are becoming one of the fastest growing ways to achieve reliable savings.
Airside economizers, in particular, aren’t just one of the most effective ways to reduce operating costs; they’re a requirement in many commercial HVAC systems throughout the United States. They also fulfill another important Indoor Air Quality (IAQ) requirement by providing the correct ratio of outside air to return air.
Until recently, most economizing solutions left a great deal of room for error. Many studies showed that while some economizers frequently experienced a wide range of mechanical issues, others simply didn’t have the capability of delivering the level of energy savings that they claimed to provide. Also, because of their complexity, many economizers presented installation complications; further reducing their ability to effectively cut energy costs.
This, however, is quickly changing as many economizers can now be customized to handle HVAC applications in specific geographical regions. Instead of offering an all-in-one solution, these products now take into account the natural climate of the location that they are being utilized in.
One of these products is Belimo’s ZIP Economizer and unlike other models that take a great deal of time and effort to setup, it can be programmed in less than a minute. Equipped with all relevant climate zone and energy code data already built in, the ZIP economizer requires only the entry of a zip code. After that, a building’s HVAC operations are automatically optimized and energy savings can be maximized with minimal interaction from the user. In addition, through use of various state and federal rebate programs, many utility providers will pay the cost of installing an economizer, which further increases their feasibility. Other benefits associated with Belimo’s ZIP Economizer can been viewed online.
For more information on Belimo’s ZIP Economizer or any more of their products, you can visit their website at https://www.belimo.us/americas/ or call them toll free at 1-800-543-9038.