Belimo Assistant 4+

BELIMO Automation AG

    • 3.8 • 10 Ratings
    • Free

Screenshots

Description

Complete transparency at all times regarding your Belimo HVAC actuator solution and the operation of your system. With the Belimo Assistant App, your iPhone provides wireless on-site operation for dampers and valve actuators. For VAV-compact actuators and trending a ZIP-BT-NFC converter is needed.

Efficient commissioning, rapid function checking during operation, handy to use and ready whenever service is required.
Simple adaptation for conversion. Document and send your setting and operating data.

The App is exclusively for use in connection with an actuator with integrated Near Field Communication from Belimo, identified by the NFC logo.

Functions
• Display identification data: device type, position, designation, serial number, MP address
• Operating data and setting parameters
• Trend view of actual data
• Send operating and setting data directly from the system, via e-mail, WhatsApp, SMS, ...
• Saving of operating and setting data on the smartphone
• NFC data transmission with deenergised actuator or during ongoing operation
• Automatic language adaptation (DE / EN / FR / IT / CN / RU / ES)
• Diagnosis page: device specific state information

Prerequisites
• Belimo actuator solution with NFC logo
• For VAV-compact actuators: ZIP-BT-NFC Converter, available at your Belimo representative
Additional information can be obtained from your Belimo representative or www.belimo.com

Using the Belimo Assistant App
• Pair your iPhone with the Converter.
• Place the converter on the Belimo Device – align to the NFC-Logo.
• Now read, modify and write Data

Notes
• The App can be installed only on an iPhone or iPad with iOS 12+.
• The App collects statistical data from Belimo devices and transmits these data to the Belimo cloud. These Statistical Data shall be processed for the purposes of future optimization and further development of the Belimo devices as part of anonymous analyses and statistical evaluations. Only data concerning the communication between the Belimo device and the app and information about the Belimo device and the device on which the app is located are transmitted which do not allow any conclusions about persons using this service.
• Actuators without NFC interface are operated with the conventional tools, see www.belimo.com

What’s New

Version 5.8.8

- Additional device profiles
- General improvements and bug fixes

Ratings and Reviews

3.8 out of 5
10 Ratings

10 Ratings

Joeynotoes ,

Very helpful

Really helpful app. I’m finally able to program and troubleshoot my actuator write on the fly get real-time data.

ALC Engineer ,

Worked great… that one time

I really need the NFC for this app to work. I have spent far too much time in the field, on top of a ladder, with my arm up in the air straining, and praying that this thing will actually connect.

Nothing like having to make a trip all the way back to the office to grab the old Belimo interface tool because this dang thing failed to work again.

For reference, I have an iPhone 12 with the latest software.

J_Scuba ,

Garbage

This don’t work on iPhone 14 PRO Max

Developer Response ,

Please contact your local Belimo representative for support.

App Privacy

The developer, BELIMO Automation AG, indicated that the app’s privacy practices may include handling of data as described below. For more information, see the developer’s privacy policy.

Data Linked to You

The following data may be collected and linked to your identity:

  • Location
  • Contact Info
  • User Content
  • Identifiers

Data Not Linked to You

The following data may be collected but it is not linked to your identity:

  • Usage Data
  • Diagnostics

Privacy practices may vary, for example, based on the features you use or your age. Learn More

Supports

  • Wallet

    Get all of your passes, tickets, cards, and more in one place.

More By This Developer

Belimo RetroFIT+
Shopping
Belimo Display
Utilities
Duct Sensor Assistant
Utilities
Belimo BEhive
Utilities

You Might Also Like

TurboTool®
Utilities
ZAset mobile
Utilities
DKN Cloud NA
Utilities
Grundfos GO - New Pump Tool
Utilities
Grundfos GO Remote - Pump Tool
Utilities
Airzone Cloud
Utilities