Belimo's FSKN remote inspection module and FS series actuators are revolutionizing the way HVAC professionals approach life safety testing. Traditionally, technicians had to manually inspect dampers by physically climbing ladders or accessing hard-to-reach areas, which was both time-consuming and costly. With the FSKN, remote testing is not only possible but streamlined to comply with NFPA 80 and NFPA 105, enabling the testing of life safety dampers without the need for visual inspections. This automation is particularly relevant for containment dampers, which need to be tested every four years in commercial buildings and every six years in hospitals.
However, despite these advancements, some life safety professionals are concerned that this shift toward automation may reduce job opportunities. What they may not realize is that this technology opens up new avenues for skilled technicians. With the FSKN’s ability to remotely monitor and test dampers through BACnet or Modbus communications, technicians can manage and service multiple buildings at once. Instead of being confined to one site for weeks to perform routine testing, they can remotely initiate tests across many locations, receive real-time reports on damper positions, and only send personnel when a problem is detected.
This shift in how periodic testing is performed allows HVAC professionals to offer new service models. By offering service agreements that include remote testing, they can provide predictive maintenance services, alerting building owners to potential issues before they become critical. This creates a proactive maintenance strategy that benefits both technicians and building managers, as problems can be addressed promptly, minimizing downtime and ensuring compliance with safety standards.
Ultimately, remote testing does not replace the need for qualified professionals. As per NFPA 80 and 105, if a remote test fails, a visual inspection must be performed. Instead, it enhances inspectors’ roles by offering them greater control, increasing efficiency, and allowing them to manage a broader portfolio of buildings. With the FSKN, the scope of what technicians can offer their customers expands significantly, creating opportunities for more dynamic service offerings based on real-time data and early problem detection.
Are you looking for HVAC training? Belimo offers unlimited access to a library of high-quality, current, and engaging HVAC video tutorials from industry experts. Participants have told us that Belimo training has given them the skills necessary to improve their HVAC skills.