ZIP Economizer Firmware Update

Belimo has recently updated the ZIP Economizer firmware (version 1.10.00). The new features include:

  • Latest Codes & Standards – CA Title 24: 2013Belimo ZIP Economizer
    Ensured all climate zones reflect new High Limit Changeover and displaying the changeover strategy per accordance with T24.
  • Automatic Damper Scaling Upon Setup
    Upon setup, the ZIP Economizer will automatically re-span the control signal range if the actual damper mechanical stroke angle is less than 90°.
  • Expanded Heat Pump Functionality
    Easier and quicker Heat Pump setup and configuration.
  • Alarm Counter
    Multiple occurrences of alarms are kept track with an alarm counter located at the bottom of the screen.
  • Alarm Time Stamp
    Alarm messages will show how long ago the alarm occurred.
  • Resettable Operation Hours
    Ensures consistency for service and repairs by resetting operation hours based on season, repairs, or energy bill periods.
  • Expanded Help Text
    Additional several help text messages with details to ensure assistance every step of the way.

Learn more about the ZIP Economizer online at www.ZIPeconomizer.com.

Back to Blog