Experience the new technology at AHR Booth 3749 offered by Belimo

Reduce Cost and Save Energy!

Visit Belimo at booth 3749 to see a live demonstration of the new Belimo Energy Valve™, a two-way pressure independent control valve that optimizes, documents and proves water coil performance.

Energy ValveWhen water coils don’t operate efficiently, energy intensive components like chillers, boilers and system pumps consume more energy than they should. Unfortunately, most owners don’t know when coils are operating inefficiently or the impact this has on system wide efficiency.  

The Belimo Energy Valve not only keeps owners and/or operators informed on coil performance, it has built-in Belimo Delta T Manager that helps operators analyze and fine tune performance under any and all conditions.  The valve communicates directly with the Building Automation System (BAS) system so operators can continuously:

  • Analyze the installed power efficiency of each and every coil
  • Document and create history reports on coil performance
  • Optimize performance using advanced algorithms

At the same time, the Energy Valve provides the same reliable, automatic, pressure independent flow control for which Belimo is famous! The Belimo Energy Valve has a schedule release date of April 2012.

Learn first hand at the AHR Expo, Booth 3749. 

Back to Blog